Display the Script Editor for a Mimic

To create a Mimic script, you need to enter the script in the Mimic Script Editor.

NOTE: If a document window displays a 'chain' icon , it indicates that it is associated with another document window. For example, an inset window maintains a relationship with the parent Mimic from which it was launched. While both of the associated document windows remain open, their title bars display a 'chain' icon. If you close the parent window, both document windows will close.

You can display the Mimic Script Editor by:

Or:

Or:

The Edit Script option is only available if the selected Mimic item has scripting enabled (see Enable the Scripting Feature on a Mimic).

Once you have displayed the Mimic Script Editor, you can create your Mimic script by typing into the Mimic Script Editor.


Disclaimer

Geo SCADA Expert 2021