Global Functions

Global functions, also referred to as 'Common functions' are functions that are available for each type of object. This means that they can be used in both Mimic scripts and Alarm Banner scripts, and as they do not reference a particular type of object, their syntax has no object preface.

Like other Geo SCADA Expert-specific functions, the Global functions provide additional functionality.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Examples of the syntax for Global functions are included in the function descriptions (listed above).


Disclaimer

Geo SCADA Expert 2021