Mimic.GoForward

The Mimic.GoForward function allows the script to navigate from a Mimic to the next display. This only applies to Mimics that are in a 'chain'.

Syntax

Mimic.GoForward()

Description

Navigates from a Mimic forward to the next Mimic in the sequence.

Arguments

None

Returns

None

The script has no effect if the current Mimic is not part of a 'chain' of Mimics. The next Mimic can only be shown if there is a sequence (the sequence is created when hyperlinks to other Mimics are selected on a Mimic).

For an example, see Go to Next Mimic in Sequence.


Disclaimer

Geo SCADA Expert 2021