StaticText.Text

The Static Text Control Object that is returned by the AddStaticText function has a Text property. The Text property represents the text that is displayed for the Static text.

Syntax

Static Text Control Object.Text = Text

Where Static Text Control Object is the name of the variable (declared in your script) that is used to store the static text Control Object that is returned by the AddStaticText function.

Description

Defines the text that is shown as static text.

Arguments

Text {string}

Defines the text that is shown as static text.

Returns

String

Example:

StaticText1.Text = "Pump 14"


Where:

  • StaticText1 is the name of the variable that stores the static text Control Object returned by the AddStaticText function
  • "Pump 14" is the text that is shown for the static text value.

Disclaimer

Geo SCADA Expert 2021