Visible

The Visible Control Object property allows the script to set the visibility of the Control Object.

Syntax

ControlObject.Visible = Value

Where ControlObject is the name of the Control Object that you are hiding/showing.

Description

Sets the position of the Control Object on the X-Axis (horizontal positioning).

Arguments

ControlObject {string}

The name of the Control Object that you want to show/hide.

 

Value {Boolean}

If set to True (1), the control is visible; if set to False (0) it is invisible.

Returns

Boolean.

For an example of how the Visible property can be used, see Mimic.Layers.


Disclaimer

Geo SCADA Expert 2021