Allocating Security Permissions

You can allocate and restrict permissions to each user account and User Group. Every item in the database can have its own set of permissions, or can be set to inherit the permissions that have been set for a parent Group or a Group Instance. The default setting for every new database item is for that item to inherit the security permissions of its parent Group (the Group that contains the item, which is the System or Root group if the item is not within a Group folder).

To allocate the security permissions for an item, you need to log on via a user account that has the Security permission for the item. Of course, the Security feature also has to be enabled on your system.

The permissions that you allocate on the Security window for a database item define which of the item's features are available to the defined users and User Groups. The permissions determine whether a user can access the features for an item, including configuration features, alarms, and controls. By allocating different permissions to different users and User Groups, you can restrict system activities.

Any item that does not have its own ACL configured (for example, a new item) will automatically inherit the ACL of its parent Group. If you want to configure an item so that it has a different ACL to that of its parent, you have to clear the Inherit Permissions from Parent check box on the Security window. The Inherit Permissions from Parent check box is selected by default, as items have the same security settings as their parent Group or the System group when they are first created.

To configure an independent ACL for an item or Group, you have to clear the Inherit Permissions from Parent check box for that item or Group. Then you can use the Permissions check boxes to configure the ACL as required.

When configuring the security permissions for a Group, you can choose whether the ACL overrides the ACLs for the items in the Group by using the Remove Explicit Permissions on Descendants feature. When you select the Remove Explicit Permissions on Descendants check box, the ACLs of the items in the Group are removed, causing the items to inherit their security permissions from the Group.

The following example illustrates how Permissions can be allocated for Group items to manage how User accounts and User Groups access various items within the database.

NOTICE

Security threat

On systems on which the 'Everyone' User Group is enabled, all User Accounts on the system automatically inherit the security permissions that are assigned to the 'Everyone' User Group, including the Guest user (which does not require a logon). Each user's security permissions comprise: Everyone permissions + User Group permissions + User Account permissions. To help avoid providing all users with unintended access to features and functionality that should be restricted, use configured User Groups rather than the 'Everyone' User Group. If the 'Everyone' User Group has to be used, it MUST be assigned the minimum permissions required, with access restricted where possible to just the relevant parts of the database. (On new installations, the built-in 'Everyone' User Group is inactive and is not assigned any security permissions by default.)
Failure to follow these instructions can result in equipment damage and a breach in system security.

Example:

This example illustrates how permissions might be allocated using User Accounts and User Groups. A typical system might contain the following set of User Groups. The 'Everyone' User Group is a built-in group.

A typical system might contain the following set of User Accounts that encompass Engineers, Operators and System Administrators.

In ViewX, it is possible for a user to have the permission to access a feature for a database item but still be unable to access the feature. This is because in ViewX a user can only access an item's feature if the item's security settings grant the relevant permissions to the user and the ViewX feature is enabled for the User.

A similar situation can occur when the Permission Restrictions settings are in place. The Permission Restriction settings override other security features and allow you to prevent just ViewX users, just Virtual ViewX users, or all system users from having access to certain features irrespective of their user account permissions. To access a feature, your user account has to have the relevant permission and that permission has to be unrestricted by the server’s Permission Restrictions settings (see Use Server Side Permission Restrictions).

Further Information

Organize your Users and User Groups.


Disclaimer

Geo SCADA Expert 2021