Define the Access Settings for Non-Secure Original WebX Connections

You can configure your system so that Virtual ViewX and Original WebX clients can access the Geo SCADA Expert database via non-secure HTTP connections (see Define the Listen Port Settings for Original WebX Clients). As HTTP connections are unsecure, potentially the communications could be intercepted and used for malicious purposes. For this reason, Geo SCADA Expert has certain safeguards in place by default:

However, in certain specific circumstances (such as testing a system), there may be a need for an engineer to log on and issue controls via an unsecure connection. To facilitate this, the Server Configuration Tool’s WebX settings include the following settings:


Disclaimer

Geo SCADA Expert 2021