Define whether a User can Access the System via ViewX, Virtual ViewX, Original WebX, or Phone

The properties described in this topic apply both to User Forms and User Pattern Forms. (User Patterns only apply to systems on which Geo SCADA Expert can create new User accounts automatically as part of an External Authentication process. For more information, see Create User Accounts from a User Pattern.)

You use the Access Type setting on the User Form (or, if applicable, the User Pattern Form) to specify which system interfaces are available to users that log on via the User account. The Access Type setting is enabled only if the Report User check box (elsewhere on this tab) is clear (see Define Whether a User Account is Used for Report Generation).

The types of system interface are:

To specify which of these interfaces are available to a user account:

  1. Either:

  2. Select the General tab.
  3. Define the Access Type settings for the user account:

    • Select the check boxes for the interfaces you want to make available to the user account.
    • Clear the check boxes for the interfaces that are to be unavailable to the user account. Users that log on via the account will not be able to log on using those types of interface.

Disclaimer

Geo SCADA Expert 2021