Export a Password Blacklist

Geo SCADA Expert provides you with the facility to export the password blacklist that is contained within a Password Blacklist item. This allows you to retrieve the list in the event the original source file has not been archived.

To export a password blacklist:

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the password blacklist item from which you want to export a password blacklist.
    A context-sensitive menu is displayed.

  3. The Export password blacklist dialog is displayed:

    This allows you to enter the location and the filename of the exported password blacklist or you can use the browse button to search for a location to save the file.

  4. Select OK to save the file. Geo SCADA Expert creates a Windows based ASCII text file containing the blacklist.

 


Disclaimer

Geo SCADA Expert 2021