Secure and Non-Secure Web Ports (Original WebX)

This topic is associated with Original WebX.

There are two types of port that you can set up when configuring the WebX settings in the Server Configuration Tool:

NOTICE

loss of communication

Ensure that the WebX configuration is not set up so that all of the following apply:
  • The Allow local connections only check box is selected in the Listen Port section of the WebX settings

  • The deprecated HTTPS Support is disabled

  • A local IIS reverse proxy is not in use.

If all of the above settings apply, then the Original WebX client will be unable to connect to the Web server. In addition certain features in ViewX and Virtual ViewX will not function correctly.

Failure to follow these instructions can result in loss of communications between Geo SCADA Expert and the Original WebX client.

Use the relevant sections of the WebX settings in the Server Configuration Tool to specify the port settings for the Web server. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021