Use Secure Web Ports with a Trusted SSL Certificate

Your Geo SCADA Expert system can be accessed via the Internet or a company intranet. To provide this functionality, Geo SCADA Expert uses web ports for both the Geo SCADA Expert web server (for Original WebX and other clients that use this web API) and for the Virtual ViewX web server. Both are accessed via local reverse proxies. The configuration of each is managed using the Windows IIS Manager tool, although the Geo SCADA Expert web server requires additional configuration within the Geo SCADA Expert Server Configuration tool to match the IIS settings. This topic focuses on the web port configuration that relates to the Geo SCADA Expert web server (for Original WebX and other clients that use this web API). Please consult Windows help for assistance in setting up IIS securely.

There are two sets of web ports:

When a web browser accesses a web server via the secure sockets protocol (HTTPS), the web browser will request the server's SSL certificate. The web browser uses the information in the certificate to:

If the deprecated HTTPS port within Geo SCADA Expert is used instead of the recommended IIS reverse proxy, then an SSL certificate has to be configured in the Geo SCADA Expert web server. In this case, if an administrative user has not already configured an SSL certificate in the web server, Geo SCADA Expert will automatically create a top-level non-trusted SSL certificate for that web server.

If a non-trusted SSL certificate (such as the server-generated one mentioned previously, or a self-signed certificate configured in IIS) is used, the Original WebX or other client will display warning messages when users access the system. The exact warning message depends on the browsers, but typically might be 'There is a problem with this website’s security certificate'. Some users may find these warning messages distracting, although they do not affect their ability to interact with your Geo SCADA Expert system.

If a trusted SSL certificate is used, the client is able to verify that it is connecting to the expected server, and so there are no warning messages shown when a client accesses the secure web server ports.

We recommend that you obtain trusted SSL certificates for your web servers as this will mean that users do not receive distracting warning messages.

Alternatively, you can either:

For more information, see the Geo SCADA Expert Knowledge Base.

We also recommend you review your security options and establish appropriate security for your web server.

Recommended security:

Increased security:

We recommend that you do not:

For more information, see Configuring Security and Connection Settings for Original WebX Clients.


Disclaimer

Geo SCADA Expert 2021