Abort a Database Backup
The topics in this section explain how to make a backup of your database at any time, typically for restoration or archival purposes. Geo SCADA Expert also has the ability to generate an automatic backup of the database whenever you upgrade the Geo SCADA Expert software on a server. This is a different type of backup.
If an on-demand or scheduled database backup is taking place and you wish to cancel it, you should use the Abort Backup action (method). Abort Backup is only available for a Backup database item when a backup is underway. When selected or triggered, it instructs Geo SCADA Expert to stop the backup.
LOSS OF DATA
(Backup Aborted) comment after the backup filename. Geo SCADA Expert will retain the aborted backup and the files that it contains. We recommend that you do not try to restore an aborted backup.
To abort a database backup:
- Run ViewX and log on via a User Account that has the System Admin permission.
- Display the Database Bar (see Display an Explorer Bar).
- In the Database Bar, right-click on the Backup item that is associated with the backup that is currently taking place.
- From the context-sensitive menu, select Abort Backup.
The Abort Backup method could also be triggered in the same way as any other method
Further Information
Logic: see Calling a Method.
Alarm Redirections: see Select the Action to be Taken.
Method Calls: see Configure the Method Call's Properties.