Geo SCADA Expert on Citrix and Remote Desktop Services

You can run Geo SCADA Expert on remote desktop setups such as Citrix XenApp and Microsoft Remote Desktop Services. (Microsoft Remote Desktop Services was formerly known as Microsoft Terminal Services.) These products allow Citrix and Remote Desktop Services clients to provide the features of a ViewX client without having ViewX installed locally.

In the following sections, we provide an overview of the Geo SCADA Expert-Citrix/Remote Desktop Services concept and also offer an insight into the pros and cons of this type of architecture:

If you decide that this type of architecture is suited to your requirements, you will need to contact a specialist Citrix or Remote Desktop Services agent for more information. The agent will:

There are no settings in Geo SCADA Expert that need to be changed specifically for use with Citrix or Remote Desktop Services. The only Geo SCADA Expert specific requirement is that a ViewX, Virtual ViewX or Original WebX client is installed/set up on the Citrix/Remote Desktop Services server(s). These clients need to be connected to the Geo SCADA Expert server in the same way as a ‘normal’ ViewX, Virtual ViewX or Original WebX client. However, your agent will need to be aware of the Requirements for Citrix XenApp or Microsoft Remote Desktop Services.


Disclaimer

Geo SCADA Expert 2021