Communications Logging Status on Status Displays

On Status displays (also referred to as View windows or View dialogs), the logging status is indicated by these entries:

To access a Status display, select the View Status option on the context-sensitive menu for a channel (either in the Database Bar, on the Channels List, or on a Mimic that contains an animated representation of the channel).

The value for these entries is one of the following:


Disclaimer

Geo SCADA Expert 2021