De-Militarized Zone (DMZ) Permanent Standby Servers

De-Militarized Zone (DMZ) Permanent Standby servers are servers that are used as an additional part of a Hot-Standby Pair or Triple Standby architecture. Like 'normal' Permanent Standby servers, they can only be set to Standby and cannot switch to Main. However, they have one key difference to 'normal' Permanent Standby servers—DMZ servers have no connection back to the system. (If the 'Allow DMZ Object Updates' check box is selected in the Partners section of the Server Configuration tool, limited credential updates and event logging of users' accesses via the DMZ are made available to be written to the Main server.) This means that DMZ Permanent Standby servers offer more protection against malicious attacks than 'normal' Permanent Standby servers. Another benefit is that as there is no connection back to the system, it makes the configuration of a firewall between the system and the DMZ Permanent Standby server a much simpler task.

DMZ Permanent Standby servers are only able to provide read-only access to clients. Any clients that connect to Geo SCADA Expert via a DMZ Permanent Standby server can be used to display data, but cannot be used to perform controls, and so on.

With a 'normal' Permanent Standby server, the Permanent Standby server can send data to, and receive data from the Main and Standby servers.

With a DMZ Permanent Standby server, the DMZ Permanent Standby server can only receive updates from the Main server (as part of the synchronization process). Any read requests are handled locally by the DMZ server itself, based on the information it has received from the Main server.

(If the 'Allow DMZ Object Updates' check box is enabled, limited credential updates and event logging of users' accesses via the DMZ, will be available to be written to the Main server.These updates are batched and made available as part of the synchronization process.)

As with normal Permanent Standby servers, DMZ Permanent Standby servers can be used:

Geo SCADA Expert allows you to connect up to four DMZ Permanent Standby servers to a Hot Standby Pair architecture or up to three DMZ Permanent Standby servers to a Triple Standby architecture. Typically, a system that uses DMZ Permanent Standby servers is set up as follows:

To set up a multi-server architecture that uses one or more DMZ Permanent Standby servers, refer to the following section:


Disclaimer

Geo SCADA Expert 2021