Define the Names/IP Addresses of the Other Servers

When you are configuring a server that is part of a multi-server architecture, you need to specify the Name or IP Address of every other server in the architecture. The server will use this information in conjunction with the Port settings to recognize the other servers.

You need to specify the Name or IP Address for every server that connects via the main connection. If a dual ethernet connection is in operation, you will also need to specify the IP Address of every server that connects via the backup connection.

The Server Configuration Tool’s Partners settings includes a Main Connection section and a Backup Connection section.

In the Main Connection section, you should define the Name or IP Address of every other server that uses the main connection to communicate with the server you are configuring.

Only configure your server to use IPv6 if your network supports it. With Geo SCADA Expert 2020 onwards, client and server-to-server connections can support the IPv6 protocol. Whereas other TCP/IP connections, such as those used by drivers, currently only support the IPv4 protocol.

If your system uses a dual ethernet connection, you can use the Backup Connection section to define the IP address of every other server that connects via the backup connection.

When you have defined the Names or IP Addresses for the Main Connection (and Backup Connection as required), you will need to define the following settings:


Disclaimer

Geo SCADA Expert 2021