Define what Action Should be Taken when a Server Becomes Isolated

In multi-server architectures, it is possible for a server to both lose its connection to other server(s) and for ICMP polls to fail. This can happen, for example, when there is a network failure. When this happens, the server becomes isolated. That is, it cannot communicate with the other servers.

When a Standby server becomes isolated, it can perform one of the following actions:

We recommend that:

When a Main server becomes isolated, it will remain a Main server. When the network connection is restored, it can perform one of the following actions:

To specify how a server should behave if it becomes isolated, you use the Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool). Select the System Configuration folder, then select Partners and then select the Miscellaneous tab.

 

Use the Action on isolated standby combo box to specify how a Standby server should behave if it loses its network connection with other servers.

Select from:

Use the Action after isolated main combo box to specify how a server should behave after a network connection is restored to an isolated Main server:

Select from:

A Main server and a Standby can both become isolated. In this situation, if the Action on isolated standby combo box is set to Go Main and the Action on isolated main combo box is set to Lose Arbitration on both servers, then arbitration will take place (see Example: Isolated Main and Isolated Standby ).

Further Information

Hot-Standby Pair Architecture

Triple Standby Architecture

Enable or Disable Duty Mode


Disclaimer

Geo SCADA Expert 2021