Enable or Disable Historic Data Storage

To allow Geo SCADA Expertto store the historic values of database items, you need to enable the Historic Data feature. However, you should only enable Historic Data if you really need to use past values as storing historic data will place a demand on your system's resources.

To enable or disable the Historic Data feature:

  1. Access the Geo SCADA Expert Server Configuration Tool.
  2. Expand the Historic Configuration branch.
  3. Select the Historic Data entry.

  4. Either:
  5. Apply the changes to the server.

When the Historic Data feature is enabled, the points, master station accumulators, and so on, can be configured to have their values stored historically in the database.

To store point or master station accumulator data historically, historic also needs to be enabled on the individual points and master station accumulators. For information, see Defining Historic Details for a Point, and see Tabs on Accumulator Forms. (Historic storage is disabled by default on new points and accumulators).

The historic values of the items are stored for a defined amount of time (see Specify the Duration to Retain Historic Data Online). At the end of the defined time, the values are deleted or archived as required (see Archiving).

If your system is only designed to monitor the current values, you should disable the Historic Data feature so that system resources are conserved.

Now that you have enabled or disabled the historic data feature, you can either proceed to configure other Historic Configuration settings (see Historic Configuration Settings) or you can continue with the server configuration.


Disclaimer

Geo SCADA Expert 2021