Troubleshooting Dynamically Assigned Ports

Geo SCADA Expert can detect remote serial communications failures on dynamically assigned ports. Any such failures are shown in the Events List which you can access from a ViewX or Virtual ViewX client.

You can also configure communications channels so that, in the event of a communications failure, Geo SCADA Expert raises an alarm. You can then view and respond to the alarm via the Alarm Banner, Alarms List, relevant Queries Lists, and suitably configured Mimics. For further information about configuring the channels for a particular driver or communications protocol, please refer to the relevant driver-specific documentation.

Each alarm or event has a message that describes the cause of the failed communications. Other topics in this section provide information about common alarm / event messages for communication failures on dynamically assigned ports. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021