Types of Extra Database Field

The configuration fields are used to contain data that relates to the setup and functionality of an item, and the data fields are used to store values.

Extra fields, with the exception of extra point data fields, are shown as columns on Queries Lists and can be included in filters.

For more information on the types of field, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2021