Using Windows Performance Monitoring Counters
            To use the Windows Performance Monitoring Counters you need to :
- Access the Windows Performance Monitor
                    
If you are familiar with this tool select Add Geo SCADA Expert Counters to the Performance Monitor for details of how to add Geo SCADA Expert counters.
 - Add the Geo SCADA Expert Counters to the Performance Monitor Counters
 - Display the Performance Monitoring Counter Data.
 
NOTE: The procedures described are for Windows 10. For other version of Windows and more detailed information about the Windows Performance Monitor refer to the Windows Help.
Further Information
Windows Performance Monitor uses performance counters, event trace data, and configuration information, which can be combined into Data Collector Sets. For more information about the Windows Performance Monitor, see http://go.microsoft.com/fwlink/?LinkId=70270.