Data File Cache

The Database branch of the Server Status Tool includes a Data File Cache category.The category shows statistical information about the data files that are used by Data Tables, Crystal Reports definition files, the latest Crystal Reports data files, and some other driver-specific files. The data that is used in the Data Tables, Crystal Reports definition files, and so on, is stored in Data Files. When the data in the files is required, the relevant data files are loaded into memory. If changes are made to the data files while they are loaded in memory, Geo SCADA Expert will attempt to flush these changes so that they are stored in the data files on disk.

The Data File Cache statistics are displayed under these categories:

Further Information

Information about the data files on the system: see Data Files.

Location of the Data Files: see Locations of the Database Folders in the Geo SCADA Expert Guide to Server Administration.

Define the Cache and Flushing settings for the Data Files: see Data Files Settings in the Geo SCADA Expert Guide to Server Administration.


Disclaimer

Geo SCADA Expert 2021