ICMP Polls

The ICMP Polls category shows the status of ICMP 'pings' between the main and standby servers. This information is useful when investigating the connections between the Geo SCADA Expert servers—if the ICMP ‘pings’ are unsuccessful, this would indicate that Geo SCADA Expert could not transmit the ‘pings’, which may be due to abnormal network conditions.

The ICMP Polls category provides the following information:


Disclaimer

Geo SCADA Expert 2021