Indices

Geo SCADA Expert database indices are used to provide faster access to specific areas of the database. For example, the point index contains the point data, so you can use it to search through the point data without having to also search through the rest of the database.

Information about the various indices is shown in the Indices category:

The status information for the database indices is shown under these headings:

The Indices status information can be used to evaluate the performance of a Geo SCADA Expert system. Typically, it is used by Geo SCADA Expert engineers to determine whether the indices are appropriate.


Disclaimer

Geo SCADA Expert 2021