Link Threads

The Link Threads category provides status information about the threads that are handling the server links.

The status information for each client is categorized under these headings:

The number of threads varies according to the size of your system.

You can use the Requests information to determine how busy the system is—if the number of requests is rapidly rising, then there may be an overload on the system and your system's performance will be affected. If your system appears to be suffering from slow performance, please contact Schneider Electric.


Disclaimer

Geo SCADA Expert 2021