Threads

The Threads category provides status information about the threads that are in use by the server. Each thread is a separate execution path within a process. For example, the DB Event thread is an execution path within the Geo SCADA Expert Database Server process. The threads allow the process to perform multiple tasks simultaneously.

Many threads are started when the Geo SCADA Expert server is started and remain for the duration of the Database Server process's lifetime. However, the usage of a thread might vary throughout the lifetime of the Database Server process. For example, on a multi-server system, threads that support a specific standby server are initialized at the start-up of the Main server, but might not be used significantly until many hours or days later when that standby server is actually started.

The status of each thread is categorized as:


Disclaimer

Geo SCADA Expert 2021