XML-DA Subscriptions

When using XML-DA to access the database, an XML-DA subscription is required. The XML-DA subscription contains information about the XML-DA tags that are being requested by a client. By using the Server Status Tool’s XML-DA Subscriptions category, you can view the status of the XML-DA subscriptions currently in use by clients (that are connected to the server.)

You can view status information about the individual XML-DA tags for each subscription in the XML-DA Items category (see XML-DA Items)

The XML-DA Subscriptions category provides the following information:


Disclaimer

Geo SCADA Expert 2021