Configure the PPI Station Parameters

When the Connection Type is set to PPI via serial adapter, use this field on the Connection tab(s) to configure the Station Parameters:



Disclaimer

Geo SCADA Expert 2021