This section is for system administrators and high-level engineers who need to use statistical and diagnostic information to assess the state of the Geo SCADA Expert system. This section applies to most simple drivers. For driver-specific information, see the individual driver guides. For more general information on analyzing a Geo SCADA Expert system, see System Analysis in the Geo SCADA Expert Guide to the Server Status Tool.
During system analysis, you might need to:
- Adjust the Configuration of any Points that Cause a High Load
- Use Driver Log File Options that are Common to Many Simple Drivers.
Additionally, if a scanner is not communicating with the server when it should be, see Troubleshooting.
When troubleshooting on a Geo SCADA Expert system, always check the Events List for diagnostic messages. These may help to identify the cause of any abnormal conditions that Geo SCADA Expert has detected.