Geo SCADA Expert Prerequisite Components

Geo SCADA Expert is designed to run on a computer that has certain other components installed. The components comprise a combination of the following:

WARNING

DO NOT UNINSTALL PREREQUISITE COMPONENTS

Uninstalling the prerequisite components may result in Geo SCADA Expert being unable to provide access to certain features, or being unable to run. It could also affect system security. For these reasons, do not uninstall the prerequisite components.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

When you install Geo SCADA Expert, the components that are essential for Geo SCADA Expert to run on your operating system are installed automatically. A prompt is displayed for non-essential components, allowing you to choose the components that are relevant to your system.

We suggest that you only choose to install components that you need for your system. For example, you only need to install the:

Installing components that are not needed on your system uses up disk space unnecessarily.

Further Information

Prerequisites for machines on which Virtual ViewX is installed: see Virtual ViewX Server Prerequisite Components.


Disclaimer

Geo SCADA Expert 2021