Run the Geo SCADA Expert Installer

To install Geo SCADA Expert on a client or a server, you need to run the Geo SCADA Expert installer program.

To run the Geo SCADA Expert installer:

  1. Insert the Geo SCADA Expert DVD. If Autorun is disabled on your PC, run the DVD manually.
  2. When the Geo SCADA Expert screen is displayed, select the Install Geo SCADA Expert option.

    The Geo SCADA Expert installer runs.

  3. When you run the Geo SCADA Expert installer, Windows may ask you if you want Geo SCADA Expert Setup to be able to make changes to your computer. Choose Yes to allow the Geo SCADA Expert installation to continue.

When you run the Geo SCADA Expert installer, it checks to see if your PC has the prerequisite components installed.


Disclaimer

Geo SCADA Expert 2021