Put the Mimic into Run Mode

To configure a Mimic, you need to display it in Design mode. But to use the Mimic in the same way as an operator level user, you need to display it in Run mode. When a Mimic is in Run mode, it will display the values and animations that have been configured for it and will provide access to any display and control related context sensitive menus. However, you cannot access any configuration features of the Mimic while it is displayed in Run mode.

To display the 'MyTestPlant' Mimic in Run mode:

With the Mimic in Run mode, you can move on to Hand Control the Internal Analog Point. The control will change the value of the point which will have a noticeable effect on the animated objects on your Mimic.

Further Information

Run Mode and Design Mode: see Displaying a Mimic.


Disclaimer

Geo SCADA Expert 2021