Welcome to the Geo SCADA Expert Tutorial

Welcome to the Geo SCADA Expert tutorial, where you will learn how to configure a variety of system features, including Mimics, database points, and connections to SCADA devices. Please note that throughout the documentation, Geo SCADA Expert is referred to as Geo SCADA Expert.

The Geo SCADA Expert Tutorial uses an Example Projects database that you can install as part of your Geo SCADA Expert installation process. You can also import the database if you have already installed Geo SCADA Expert. The security features built into Geo SCADA Expert require either a Super User or System Administrator to enable the example user accounts. You require these user accounts to follow the tutorial examples, see Example Projects in the Geo SCADA Expert Guide to Installation, for information about how the database is installed and the user accounts enabled.

Intended Audience

This tutorial is designed for use by users who are new to Geo SCADA Expert. By following the procedures in this tutorial, users can learn about a variety of Geo SCADA Expert interfaces, concepts and features.

After completing the tutorial, users will be familiar with many of the key aspects of Geo SCADA Expert. They will also have an appreciation of the many benefits a Geo SCADA Expert system offers.

Document Scope

This tutorial provides a brief introduction to a variety of Geo SCADA Expert features, including the Database Bar, Mimics, Trends, and configuration Forms.

When your Geo SCADA Expert demo system first runs, the ViewX client interface is launched automatically. You need to log on using one of the example User accounts provided to access the items within the Example Projects database. ViewX is the full client interface for the Geo SCADA Expert system and it can be used to:

ViewX is designed to reduce the amount of time and effort required to configure and maintain a SCADA system. To achieve this, it uses an innovative grouping system that works in a similar way to folders in Microsoft® Windows.

Database Bar showing Group structure, similar to Windows Explorer

The folders system offers many benefits over traditional tag table interfaces:

Designed to help first-time Geo SCADA Expert users, this tutorial explains how to use some of the many features of the two main Geo SCADA Expert user interfaces—ViewX and Virtual ViewX. The tutorial is divided into separate sections, each of which contains easy to follow instructions and helpful explanations that show you how to:

We recommend that you read the topics that are listed in the gray footer section at the bottom of this topic before you start. In addition you should refer to the Example Projects Database.


Disclaimer

Geo SCADA Expert 2021