Configuring TBox Analog Points

The TBox driver supports Analog Input Points and Analog Output Points. (For Historical Analog Points, see Configuring TBox Historical Analog Points.)

Configure the properties for each Analog Point using the fields on the TBox Analog Input Point Form or the TBox Analog Output Point Form, as appropriate.

This section covers configuration of properties on the Analog Point tab of each Form, and the properties on the Control tab of the TBox Analog Output Point Form. For information on the fields on other tabs, seeTabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.

For TBox Analog Input or Analog Output points, use the Analog Point tab to:

For TBox Analog Output Points only, there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to define properties relating to control of equipment:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).


Disclaimer

Geo SCADA Expert 2021