System Analysis

This section is for system administrators and high-level engineers who need to use statistical and diagnostic information to assess the state of the Geo SCADA Expert system. This section applies specifically to the TBox driver. For more general information on analyzing a Geo SCADA Expert system, see System Analysis in the Geo SCADA Expert Guide to the Server Status Tool.

During system analysis, you might need to:

Additionally, if an RTU is not communicating with the server when it should be, see Troubleshooting in the Geo SCADA Expert Guide to Advanced Drivers.

When troubleshooting on a Geo SCADA Expert system, check the Events List for diagnostic messages. These may help to identify the cause of any abnormal conditions that Geo SCADA Expert has detected.


Disclaimer

Geo SCADA Expert 2021