Scanner Configuration

The Totalflow-specific configuration settings for the Totalflow Scanner object are on the Scanner Options tab. There are also additional configuration fields that do not appear on the configuration form, but do appear in the schema (Scanner Configuration Fields).

To configure a Totalflow Scanner display the Properties window for a Totalflow Scanner item and select the Options tab.

Complete the following fields:

Further Information

Channel Configuration


Disclaimer

Geo SCADA Expert 2021