Introduction to the Geo SCADA Expert Translation Dictionary

Intended Audience

This guide is designed for system administrators who are setting up and managing a Geo SCADA Expert Translation Dictionary.

Document Scope

This guide describes the Geo SCADA Expert Translation Dictionary. There are two types of dictionary: The File Translation Dictionary and the In-Database Translation Dictionary. For information about the In-Database File Translation Dictionary, see the Geo SCADA Expert Guide to the In-Database Translation Dictionary.

About the Geo SCADA Expert Translation Dictionary

You can replace user-created text in Geo SCADA Expert with text translations. To do this, you create a Translation Dictionary which contains the user-created text items and associated translated text. You then mark the user-created text in Geo SCADA Expert that you want to replace and Geo SCADA Expert will perform a search and replace using the Translation Dictionary.

For example, you might want to replace text in a Mimic with a translation of the text in another language. In Geo SCADA Expert, you mark the text you want to replace with a @ prefix. Geo SCADA Expert will then search for the marked text in the Dictionary, retrieve the translated text associated with it, and then replace the marked text with the translated text.

You can use the Geo SCADA Expert Translation Dictionary in the following:

In Geo SCADA Expert, you can create two different types of Translation Dictionary. However, you can only use one type of Dictionary at a time. You can use either of them to perform the search and replace for marked text. However, the two Dictionary types differ in how you create and maintain them and how they are integrated with the Geo SCADA Expert database. The two types are as follows:


Disclaimer

Geo SCADA Expert 2021