Display Continuous Data

You can set a Trend to display the next interval automatically when the current time exceeds the time shown on the X-Axis. When you have set the Trend to work in this way, the Trend is updated to show the latest interval so that you can see the current time.

To display continuous data on a Trend:

  1. Right-click on the X-Axis.
    A context sensitive menu is displayed.
  2. Use the Continuous option to toggle the continuous data mode on and off. If the check is shown, the continuous data mode is currently enabled.

Disclaimer

Geo SCADA Expert 2021