Display a Trend in Run Mode

Operator level users (users that operate the system rather than configure it) use Trends in Run mode. When you display a Trend in Run mode, you have access to the navigation features and can use them to view and compare the data on the Trend.

On a ViewX client, security permissions and menu options determine whether you display Trends in Run mode or Design mode.

On a Virtual ViewX client, you can only display Trends in Run mode.

How you display a Trend in Run mode depends on the type of Trend. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

If your User account provides access to Favorites, you can use the Favorites bar to display any Trends that you have previously added to your Favorites list. For more information, see Use the Favorites Bar to Access your Favorites.


Disclaimer

Geo SCADA Expert 2021