Min

The Min algorithm works in the same way as the Max algorithm except that it calculates the lowest value in a sample rather than the highest.

For information on the Max algorithm, see Max.


Disclaimer

Geo SCADA Expert 2021