Optional Value Types and Assignments

You need to assign each Optional Value a value of the appropriate type, using the appropriate syntax. The topics in this section explain the syntax that you need to use for each type of value. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

The tables in the topics indicate the type of value that each optional identifier supports and provide examples of the values that you can specify.


Disclaimer

Geo SCADA Expert 2021