Supported AggregateId Values

With a trace that displays processed historic data, use the AggregateId identifier to define the algorithm that Geo SCADA Expert uses to process that historic data. TrendSpec’s AggregateId identifier is equivalent to the Algorithm property on pre-configured Trends (see Configure a Trace).

Take care with End and End Last Historic Algorithms used on clients, or with Geo SCADA Expert features, that run in Local Time with Daylight Saving Time. Ensure that the start and end times specified for the sample interval do not coincide exactly with the time at which the clock jumps backward. Include a small offset in the sample time, to offset the calculation to avoid the sample end or start time exactly matching the time that the clock jumps backward at the transition from Daylight Saving Time to Standard Time. A small offset of 1s or even 1ms should suffice. For more information about Daylight Saving Time, see The Effects of Daylight Saving Time Adjustments.

To specify the algorithm that Geo SCADA Expert is to use when processing historic data, you assign the SOURCE’s AggregateId the appropriate long value.

If a TRACE’s Interval identifier is set to a specific time period, you can assign the corresponding SOURCE’s AggregateId any one of a number of long values, including:

Long Value

Algorithm

Long Value

Algorithm

1

Interpolated

20

DurBad

2

Total

21

PerGood

3

Average

22

PerBad

4

Time Average

25

Sum

5

Count

26

24hAverage

6

StdDev

27

8hAverage

7

MinTime

28

1hAverage

8

Min

29

Stepped

9

MaxTime

30

Min Last

10

Max

31

Max Last

11

Start

32

Average Last

12

End

33

Min Interpolated

13

Delta

34

Max Interpolated

17

Variance

35

Average Interpolated

18

Range

36

End Last

19

DurGood

37

Moving Range

If the TRACE’s Interval identifier is set to PerPixel, the long value that you can assign to the SOURCE’s AggregateId is limited to one of the following:

Long Value

Algorithm

Long Value

Algorithm

3

Average

32

Average Last

8

Min

33

Min Interpolated

10

Max

34

Max Interpolated

30

Min Last

35

Average Interpolated

31

Max Last

---

---

Example:

A ‘custom’ ad hoc Trend is to show a trace of processed historic data.

The TrendSpec definition’s TRACE section includes this configuration:

Interval = ‘15M’

The SOURCE section within the TRACE section includes:

AggregateId = 3

This results in the trace showing the mean average value that Geo SCADA Expert retrieved from the data source during each 15-minute interval. (AggregateId = 3 triggers Geo SCADA Expert to calculate the mean average from the raw data values that it retrieved during each resample interval.)

Further Information

AggregateId identifier: see SOURCE Optional Values.

Historic algorithms used on Trends: see Built-In Historic Algorithms for Processed Historic Data.


Disclaimer

Geo SCADA Expert 2021