View Information about All Annotations on a Trace

You can use the View option to display information about the annotations that have been inserted on a Trend. This is useful when you need to view specific details about a certain annotation, for example, the name of the user that created an annotation.

To display information about the annotations on a trace:

  1. Right-click in the main display area on the Trend.
    A context sensitive menu is displayed.
  2. Select the Annotations option.
    A further menu is displayed.
  3. Select the View option.
    The Annotations window is displayed.

    View Annotations

    The Annotations window provides information about the annotations for each trace. You can use the Trace combo box to select a different trace as required.

  4. Select the Close button to close the Annotations window.

Disclaimer

Geo SCADA Expert 2021