Specify the Channel with which the Radio is Associated

Use the Channel field on the Radio tab to specify the Simple Trio Diagnostics Channel that is used for communications with this radio (either directly, via a ‘base’ radio, or through a Terminal Server or similar device).


Select the field’s browse button to display a Reference browse window, then select the required channel from the window.


Disclaimer

Geo SCADA Expert 2021