Trio Radio Series Supported by the Simple Trio Diagnostics Driver

You can use Geo SCADA Expert's Simple Trio Diagnostics driver to retrieve diagnostics data from several series of Trio radio. The type of diagnostics data that Geo SCADA Expert can retrieve from each radio varies, depending on the radio series and the type of radio unit.

The Simple Trio Diagnostics driver provides support for retrieving diagnostics data from the following series of Trio radio:

Trio Radio Comments

D Series

D Series radios are capable of providing feedback on fewer diagnostics parameters than other radio series supported by the Simple Trio Diagnostics driver. You can retrieve each of the diagnostics parameters using Simple Trio Diagnostics Analog points.

D Series radios provide a subset of other features supported by later series of Trio radios.

E Series

The E, J, K, and M Series of Trio radios use a diagnostics protocol that provides additional functionality to D Series radios.

The actual items of diagnostics data that can be retrieved from each radio vary, depending on the radio series and type of unit (for example, a base station, repeater station, or remote data radio).

J Series

K Series

M Series

Further Information

Supported System Setups.


Disclaimer

Geo SCADA Expert 2021