Acknowledge with Comment

Associated with: Any item for which an alarm can be raised

Security permission required to access this option: Acknowledge Alarms

Use this option on the Object Menu to add a comment to the Event Journal when Geo SCADA Expert acknowledges any unacknowledged alarms on the selected item, Group or Group Instance (and in any subgroups within that Group or Group Instance).

For more information, see Acknowledge an Alarm with Comment.

Also see Acknowledge Alarms.


Disclaimer

Geo SCADA Expert 2021