Context-Sensitive Menu (Document Tab)

A context-sensitive menu is displayed when you right-click on the tab of a document that is open in the document display area.

The options that are available vary depending on the current layout, such as whether you are displaying a single or multiple documents, and whether the selected document is floating or docked.

The menu options comprise a combination of the following:

Further Information

Display different text in a document tab: see Configure an Alternative Name for a Database Item.

Float or Dock Windows.

Explorer Bars.

Arrange Multiple Document Windows in the Document Display Area.

Use commands on the ViewX ribbon to close documents: see View Tab.

List all documents that are open: see View Tab.

List, and optionally 'pin', recently displayed documents: see File Menu.


Disclaimer

Geo SCADA Expert 2021