Display Data

Associated with: Table and Grid objects, such as Data Grids, Data Sets, Data Set Rows, and Data Tables

Security permission required to access this option: Read

The above mentioned database items are used for adding 'custom' tables to the database. Use the Display Data option to display the resultant data as a List.

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.


Disclaimer

Geo SCADA Expert 2021