Display Help View

This option is only available if:

Use the Display Help View option to display the ‘file object’ (such as a Mimic or Trend) that is configured as the item or Group’s Help View.

The Help View should provide help about the item or Group. For example, operating instructions for a piece of equipment.

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.

Also see Display Default View, and see Display Alarm View.


Disclaimer

Geo SCADA Expert 2021