Display Historic List

Associated with: Points and master station accumulators that have Historic logging enabled

Security permission required to access this option: Read

Select this option on the Object Menu to display a List of historic values for the selected point or master station accumulator (see Historic Lists).

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.


Disclaimer

Geo SCADA Expert 2021